Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Slide 25
Slide 26
Slide 27
Product List
This slideshows a waveform of the STK681-332 when the current limit operates. The peak of the waveform is 8.5 A; however, the peak braking current of the STK681-332 and 352 is 12 A. The higher braking current allows the motor to stop faster.
PTM Published on: 2012-11-30