Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List

Portable Medical Solutions Slide 5Shown in this slide and the next slide is TI’s broad embedded portfolio. The MSP430 has clear advantages as it is able to address most of the needs of portable medical devices. The MSP430 has the low power required, the efficient architecture and instruction set, the integrated analog, and a large range of devices to offer which makes it appealing to customers.

Shown in this slide and the next slide is TI’s broad embedded portfolio. The MSP430 has clear advantages as it is able to address most of the needs of portable medical devices. The MSP430 has the low power required, the efficient architecture and instruction set, the integrated analog, and a large range of devices to offer which makes it appealing to customers.

PTM Published on: 2011-09-09