Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Portable Medical Solutions Slide 11

Some of the available packaging options are shown in this slide. This is a wide range, and will give customers a lot of flexibility. Many times if a customer is considering smaller PCBs, it may be beneficial to select an 80-pin BGA or 113-pin BGA package or even a die-size BGA package (DSBGA), which are as small as 3.2 mm by 3.2 mm. Of course, there are trade offs with such a small package size; more board layout complexities due to routing in tighter spaces. But if a customer needs it, TI can even offer many MPS430 devices as bare die.

PTM Published on: 2011-09-09