Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Portable Medical Solutions Slide 17

Some of the applications that the PaLFI enables are shown in this slide. These include, for example, a smart pill that a person ingests to monitor the acid pH in the GI tract, and the base station. As the reader/writer is brought near the smart pill, it sends the data over to the base station. Developers now have the capability of configuring implantable devices or getting information from implanted devices from inside the body, including hearing aids, creating many different applications and innovations that this technology can enable.

PTM Published on: 2011-09-09