Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
st vs comp
Among the products in the 50 V DMOS STAC® series, the STAC4933 is specifically designed for industrial applications with stringent robustness requirements. Safe operation of the STAC4933 is guaranteed by one of the industry’s highest breakdown voltages, which is greater than 200 V, a higher load mismatch capability, which is 65:1 in all phases, and by specifying the avalanche energy at 1.2 joules, which is the parameter controlling the self-biasing of the parasitic transistor.
PTM Published on: 2014-03-26