Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Slide6
Here is an updated chart showing the various lumen ranges in cool and warm white for each member of the CXA Family. As mentioned previously, the CXA Family enables a wide range of lumen options from a couple of hundred lumens up to 10,000 lumens. Within the CXA 25 Series, lumen options are available between 2000 and 8000 lumens all in the same source and package size.
PTM Published on: 2012-11-27
PTM Updated on: 2023-01-19