Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Slide26
In summary, there are many advantages to utilizing an integrated LED array solution compared with using individual discrete LEDs that are detailed in this presentation. The CXA Family enables a full range of system designs from 300 lumens to over 10,000 lumens. The CXA Family can replace incumbent solutions ranging from a 25 watts Halogen spot light to a 175 Watt Metal Halide based fixture. The CXA Family has excellent long-term performance data across the entire product family. The CRI 95 versions of the CXA enable compelling halogen replacement solutions. There are a large variety of CXA connector solutions available from several difference sources. The CXA Family is available in a full range of color temperatures and color performance options.
PTM Published on: 2012-11-27
PTM Updated on: 2023-01-19