Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Slide19
Here are the Standard Order Codes for the CXA1507. There are several flux options, color temperatures and CRI options available from 2700 Kelvin to 5000 Kelvin. Cree have provided flux values at various temperatures and drive currents so users can make an accurate comparison when comparing the CXA 1507 to other potential solutions.
PTM Published on: 2012-11-27
PTM Updated on: 2023-01-19