Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Slide3
Here is a visual example of how one LED Array package can enable a wide range of designs. As shown in the graphic, the small optical source size enables flood, narrow flood, and spot applications utilizing the same source size, and in with the example of Cree LEDs, there are several lumen options utilizing the same source size.
PTM Published on: 2012-11-27
PTM Updated on: 2023-01-19