Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Slide 25
Slide 26
Slide 27
Slide 28
Slide 29
Product List
Biasing by logic is easily accomplished and it is recommended that an OC or CMOS device be used to guarantee turnoff. In this case, nominal IF is between 2 and 20 mA and the designer must be aware of leakage causing an “on” state since 0.5 V at 200 uA can turn it on. Therefore, use a low current to turn on the device and allow better control of the output current. Additionally, the amount of current supplied determines the speed of turn on.
PTM Published on: 2009-03-27