Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Slide 25
Slide 26
Slide 27
Slide 28
Slide 29
Product List
A normally-off type SSR (which is functionally the same as a “make contact” mechanical relay) leaves the output terminals open if there is no input signal, and short-circuits the output terminals if an input signal above threshold level is applied. Conversely, a normally closed type SSR (which is functionally the same as a “break contact” mechanical relay) keeps the output terminals short-circuited if there is no input signal, and opens the output terminals upon correct application of an input signal.
PTM Published on: 2009-03-27