Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Product List
In summary, VeriSafe is the only product currently available that provides active testing to confirm de-energized state. It verifies the installation and has safety functions that meet IEC 61508 (SIL 3). The Panduit Verisafe is listed as an AVT per UL 1436 and meets the requirements for installed testers NFPA 70E-2018 120.5 (7) Exception 1. Due to its advanced features and strong certification status, VeriSafe is a unique product of its kind in the market and delivers real value to industrial customers.
PTM Published on: 2017-08-01