Shown on this slide is the process for selecting an input topology from the menu box located at the top left of the window. Select single ended or differential input by clicking on the radio button. When this is done, the schematics re-adjust; node voltages and waveforms will recalculate automatically. Next, select input coupling by clicking on the AC Coupled1 if available or AC Coupled2 buttons. Again, the schematics re-adjust; node voltages and waveforms recalculate automatically. Automatic recalculations hold value of Rg and system gain constant, other resistor values, noise and distortion are recalculated.