Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
RFID Technology and Applications Slide 18

In addition, LF tags can survive harsh conditions such as marathon races. The tags are fastened to the competitors' shoes to record the individual's times as they pass the finish line. In fitness centers, RFID tags are also used to access individual lockers, changing rooms, and pool areas. The tags can be placed on key chains, clip-on IDs, or access cards. The durability of the cards allows people to clip the tags onto their bathing suits and wear them in the pool. Another demanding use is in waste management. Many countries have begun tagging waste containers and charging by weight to reduce land fill.

PTM Published on: 2012-09-06