Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
RFID Technology and Applications Slide 10

The magnetic coupling in LF systems is very similar to how a transformer works. The primary and secondary windings are the reader's and tag's antennas. However, RFID systems use air in place of a ferrite core and the windings are separated by a much wider distance. Nevertheless, the principles are the same. The antennas transfer power and signals by creating changing magnetic fields which induce voltages in a coil of wire.

PTM Published on: 2012-09-06