Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
CPC-Slide5

CPCs can utilize multiple types of signal contacts as well as multiple types of power contacts. The Mini Universal MATE-N-LOK contacts are industry standard contacts that are used in the Miniature CPC connector. Please note that all contact ratings are based on a single contact, outside of the housing, in ideal conditions. There are multiple factors that can affect the maximum current rating for contacts, such as housing size and the gauge of the wire that a contact is terminated to. 

PTM Published on: 2015-09-24