Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
CPC-Slide15

The Mil-C-5015 style connectors are a lighter weight and lower cost alternative to metal shell connectors in an existing system. This style of CPC is designed specifically to be used only with the metal-shell Mil-C-5015 connector systems. The Mil-C-5015 style CPC connector utilizes a special Multimate Type III + Mil-C-5015 style contact that can only be used in this specific housing due to the increased contact length. Mil-C-5015 style CPC connectors come in only two shell sizes.

PTM Published on: 2015-09-24