Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Mix Decay Function

When the motor current decays, the followability of the current will worsen depending on the current regeneration mode (Slow/Fast Decay), causing vibration and noise. As a countermeasure, a Mix Decay function is built in that externally adjusts the ratio of Slow Decay and Fast Decay during current attenuation. Reducing vibration created by a noisy waveform can be critically important in sensitive applications such as printing, where the printer head needs to move uniformly across an object or surface without incurring the distortion that can result from jerky motor movement.

PTM Published on: 2021-01-08
PTM Updated on: 2021-02-18