Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
WiFi Modules Overview Slide 9

ST makes four different families of modules right now. They have the classic Bluetooth 3.0 modules, the SPBT 632 family, Class 1 and Class 2. Those are in full production. Bluetooth 4.1 modules have started production in the third quarter of 2015. The SPBTLE-RF module that is in production has Nucleo shields available today. WiFi modules are in full production. Additionally, there are two different sub-gigahertz modules. There is the SP1ML family, which has an STM32 onboard, and the SPSGRF module, which is basically the Spirit device on a module by itself with an antenna and balun. So users have two different options for the sub-Gigahertz with and without a microcontroller. All of these modules have FCC certification for ease of design for the customer.

PTM Published on: 2016-02-01