Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
SPIRIT1 RF Transceiver Overview Slide 4

The STMicroelectronics SPIRIT1 is a flexible, low-power proprietary sub-1 GHz transceiver with integrated packet handler. SPIRIT1 can work in several frequency ranges from 150 MHz up to 956 MHz. It also supports several modulation schemes: the classic FSK, GFSK, MSK, also the older OOK and ASK. Other important features include a data rate of up to 500 kbps; power management featuring an integrated SMPS that allows further reduction of power consumption and minimizes the component count on the board. Some important definitions are: Frequency-Shift Keying (FSK) is a frequency modulation scheme in which digital information is transmitted through discrete frequency changes of a carrier wave. Gaussian Frequency-Shift Keying (GFSK) is a type of frequency shift keying modulation that uses a Gaussian filter to smooth positive/negative frequency deviations, which represent a binary 1 or 0. In a GFSK modulator, everything is the same as an FSK modulator except that before the baseband pulses (-1, 1) go into the FSK modulator, it is passed through a Gaussian filter to make the pulse smoother, limiting its spectral width. In digital modulation, Minimum-Shift Keying (MSK) is a type of continuous-phase frequency shift keying that was developed in the late 1950s and 1960s. Similar to OQPSK, MSK is encoded with bits alternating between quadrature components, with the Q component delayed by half the symbol period. However, instead of square pulses as OQPSK uses, MSK encodes each bit as a half sinusoid. This results in a constant-modulus signal, which reduces problems caused by non-linear distortion. In addition to being viewed as related to OQPSK, MSK can also be viewed as a continuous-phase frequency shift keyed (CPFSK) signal with a frequency separation of one-half the bit rate. On-Off Keying (OOK) is the simplest form of Amplitude-Shift Keying (ASK) modulation which represents digital data as the presence or absence of a carrier wave. In its simplest form, the presence of a carrier for a specific duration represents a binary one, while its absence for the same duration represents a binary zero. ASK is a form of modulation that represents digital data as variations in the amplitude of a carrier wave.

PTM Published on: 2013-02-27