Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
evolution
Phase change materials have historically been offered in sheets and preforms cut to specification. However, the latest PCTIMs are dispensable and printable liquids. This allows them to offer complete flexibility in application and thickness. Here is an example of a honeycomb pattern used to provide uniform thickness and optimized paths of air escape during wetting.
PTM Published on: 2013-07-03
PTM Updated on: 2017-06-14