Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Product List
The advantage of PCTIM is that it offers 100% wetting at the interface and virtually zero interfacial thermal resistance. As the compound goes from solid to liquid, it expands 16% in volume. This forces out entrapped air and eliminates voiding. The material shrinks back to the interface when it cools, preventing pump-out.
PTM Published on: 2013-07-03
PTM Updated on: 2017-06-14