Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Product List
Thermstrate is one of the first PCTIMs developed in the 90s. This material features a thermally conductive phase change material coated on aluminium substrate. The material melts at 60°C, providing excellent wetting and heat dissipation. Note that this material is not electrically insulating.
PTM Published on: 2013-07-03
PTM Updated on: 2017-06-14