Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
psx
Powerstrate Xtreme has proven itself to be a solid solution for removing heat. This state-of-the-art phase change material has the highest thermal conductivity (3.4 W/m*K) with phase change temperature of 45°C. This material uses aluminium powder for high conductivity, so it is not electrically insulating.
PTM Published on: 2013-07-03
PTM Updated on: 2017-06-14