Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
VLISI-Slide18

A free graphical user interface is available to program the parameters and operating characteristics of each channel as needed. An I²C communications link also allows direct control by a system microcontroller or microprocessor if desired. It is also possible to add features, flexibility and functions which are either difficult or not possible using traditional analog methods while realizing  SKU reductions and inventory concerns.”

PTM Published on: 2011-06-15