Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
VLISI-Slide11

Network processors are already requiring adaptive voltage power supply methods with multiple supply rails which are sequenced and slew rate controlled. This device has the interface to connect directly to the power supply for dynamic control, in fact it will not work properly without continuous communications and control of the power system to modulate not only the eight rails required by the processor itself, it also controls other power supply rails for memory, I/O and other system functions.

PTM Published on: 2011-06-15