Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
AmplifierProblem-Slide8

In this example the engineer is amplifying a 1V differential signal with a gain of four and is expecting a 4V output signal. The power supply is a signal ended 5V source connected to the Vcc pin, with the ground connected to the negative supply pin.

PTM Published on: 2010-12-16