Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
RG-Slide6

Different thickness of thin film is used for different resistance values. It is typically expressed using sheet resistance, Ohms/square. In Susumu’s standard NiCr alloy film, this is less than 100 Ohms/square. For high resistance RG series, they use the high resistance film with sheet resistance over 500 Ohms/square.

PTM Published on: 2017-05-23