Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Stepper Fundamentals Slide 5

The circuits required to drive each of the configurations are shown here. The Bipolar motor needs 8 transistors connected in a dual H-Bridge configuration to drive the motor while the unipolar motor needs only 4 transistors connected to ground. Early applications of stepper motors often used the unipolar configuration since it required fewer transistors to drive and did not require a level shift to drive the upper transistors of an H-bridge. So if the unipolar motor is much easier to drive, why would a bipolar stepper motor be used?

PTM Published on: 2011-12-14