Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Stepper Fundamentals Slide 2

The basic configuration for the stepper motor includes a permanent magnet on its rotor and coils on the stator. A rotating magnetic field is generated by applying alternating positive and negative currents to the stator coils. The most common configuration of a stepper motor in use today is a two phase bipolar driven motor. This motor needs an H-Bridge to drive each of the two phases. The stepper is a synchronous machine and the rotational speed is directly controlled by the rate at which the currents in the stator are changed.

PTM Published on: 2011-12-14