Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Stepper Fundamentals Slide 48

In summary, stepper motors are ideally suited for applications that require precise position control such as computer peripherals or numerically controlled machine tools. The two common configurations for stepper motors include bipolar and unipolar, and use half-step, full-step, or microstepping driving techniques. Each driving circuit will consist of the step time and phase generator (which is usually done in a microcontroller), the PWM current control, and the power bridge. Finally, when creating a stepper motor driver, the designer must consider the speed-torque performance of the motor.

PTM Published on: 2011-12-14