Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Stepper Fundamentals Slide 20

This chart shows a comparison of a typical 5V, 1A motor driven from 5V in the L over R configuration, and a motor driven in the L over nR configuration using a series resistance equal to 4 times the motor coil resistance and 5 times the drive voltage, or 25V. The rise time is significantly reduced so it would be expected to be able to operate at higher speed. However, the additional dissipation in the added external resistance is not acceptable in today’s applications. What is needed is a drive that provides a faster rise time without the dissipation of the L over nR drive.

PTM Published on: 2011-12-14