Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
DDR3 DRAM with ECC Slide 12

In summary, error rates are a significant concern in many applications. Conventional ECC solutions tend to have drawbacks in that extra DRAM has to be added, with added data lines and extra software on the processor or FPGA. In-DRAM ECC provides an advantage by removing these additional requirements. ISSI offers DDR3 with and without ECC, with temperatures up to 125°C.

PTM Published on: 2016-10-06