Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Slide4

The PMC series offers complete power supply protection features such as overload, overvoltage, short circuit and over temperature. All the products come with universal AC input encased in a full corrosion resistant Aluminum casing. Another excellent feature seldom found in the same product type is that the PMC series does not have power de-rating across the entire input voltage range. This enables full load output with very low input voltage.

PTM Published on: 2016-08-08