Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Slide16

The series can start up at very low input voltage and without any de-rating across entire input voltage range. This means full load output with very low input voltage. Competitors A and B can only start up at higher input voltage, where competitor A has de-rating and competitor B is a more expensive brand.

PTM Published on: 2016-08-08