Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Slide10

Rugged & Intelligent design is exemplified by providing full length support under the PWBA where the terminal block is mounted. This can prevent the possibility of field failure caused by excessive bending of the PWBA when too much force is applied on the terminal block during wiring. The Delta design prevents damage to the solder joints that connect the terminal block to PWBA.

PTM Published on: 2016-08-08