Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Slide8

There are a few differences between the XP and the XP2. First, as mentioned previously the dome height is slightly higher, on the new generation of XP Family. In the vast majority of designs the slightly larger dome size will have no effect on designs either physically or optically. There is also a cosmetic difference in that the XP2 family does not have the green solder mask that the original product had, as can be seen in the picture shown here.

PTM Published on: 2012-11-06