Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Slide3

This slide shown here, has where the XP2 LEDs are positioned relative to the original XP LEDs as well as other discrete Cree LEDs. The XP-E2 LED delivers similar performance as the XP-G and XT-E, at a cost that is lower than the original XP-G. The XP-E2 LED provides drop-in ready enhancements to existing XP-G and XP-E designs. The XP-G2 LED delivers better performance than the XP-G LED. The XP-G2 LED provides drop-in ready enhancements to existing XP-G designs. 

PTM Published on: 2012-11-06