Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
PowerVerter APS Inverter Chargers Slide 9

Tripp Lite APS inverter/chargers are the most reliable source for AC power, regardless of operating conditions. They have three main components: 1) an inverter, 2) a battery charger, and 3) power conditioning components such as a surge/noise filter and frequency-control circuits. When AC power is present, the inverter/charger automatically passes conditioned power through to connected equipment: blocking potentially damaging power surges, filtering disruptive line noise (which can help improve audio/video performance) and regulating frequency (which can help equipment perform at their peak). While passing through conditioned power, Tripp Lite inverter/chargers also simultaneously charge a connected battery bank, preparing it for use when power is absent. When power is absent, the inverter/charger converts DC power from the connected battery bank into AC power to support connected equipment - automatically and without interruption. Battery runtime is determined by the total amp-hours and condition of the user-supplied batteries.

PTM Published on: 2015-08-10