Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Product List
TI's Sensor AFE Development System includes a Sensor AFE IC, design and configuration software. The development system easily interfaces with sensors and the designer’s PC. The software included with the development system is the same software as in the WEBENCH® Sensor AFE Designer, so designers have the same capability to configure or modify the sensor signal path as they do with the online software. Configuration data can be downloaded to the Sensor AFE IC and designers can evaluate performance of the completed signal path, including the sensors. The development system software includes an analysis mode. The system also has the capability to compile data and generate an output such as a histogram as well as the capability to monitor an input and show signal value over time. This is called the oscilloscope mode. The system also allows designers to capture the data to a file so it can be analyzed using their own software.
PTM Published on: 2011-02-01