Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
High EMI Immunity Op Amp Lineup

Displayed here is the EMARMOUR™ lineup. The graph at the top shows the comparison results of the radio wave emission test, with the horizontal axis representing frequency and the vertical axis indicating output fluctuation. The red line is ROHM’s product. The customer can see that ROHM’s op amp operates stably in all frequencies with no output fluctuation compared to the competitor products. Both bipolar products with a wide supply voltage range and CMOS types with low bias current are offered in a variety of packages.

PTM Published on: 2023-12-14