Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
which 6
Finally, the size of the device is defined by the space on the device. Thermal and optical design might play a role too if the customer needs space for secondary optics. For instance, smaller devices sometimes deliver more optical power than larger devices. Nevertheless, if one has decided to move on with an SMD device, the largest product selection is OSLON. The SYNIOS is the smallest available package for high power.
PTM Published on: 2018-02-20