Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
zx-slide7

Improved electrical characteristics are key factors to the ZX series. Contact resistance has been lowered from the Mini-USB’s 50mΩ max down to 30mΩ max. Even after a 10,000 cycle test, the ZX series contact resistance only has a 10mΩ maximum rise. Additionally, current capacities have also been improved. Current capacity is 1A if just sending signals through contacts 1-5. However, by sending power and signals through the ZX series, current capacity is increased to 1.8A for pins 1 and 5 with a signal current capacity of 0.5A for pins 2, 3 and 4.

PTM Published on: 2015-02-02