Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
zx-slide27

Finally, temperature rise should be considered when using a connector for any power charging situations or applications. When running the higher 2.5 amps of current in the ZX series, the temperature rise is still well below 25C. The ZX series can handle 1.0, 1.5, 2.0, and 2.5 amps (depending on the configuration) when using pins 1 and 5 for power. Signal lines (2, 3, 4) will still only be carrying 0.5 amps. 

PTM Published on: 2015-02-02