Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
zx-slide23

This eye pattern here is being generated with a 1 Gbps signal and the same 2.4m cable. Although the eye pattern is not as open as with the 480 Mbps, it is still a good pattern given the frequency being applied.

PTM Published on: 2015-02-02