Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
wizard config Power Module Wizard login
This is the schematic page. Note that the values of all the external components, chosen on the previous design consideration page, are included in this schematic page. At this point, a user can float the mouse over any external component and change its unique attributes to reflect the user's on-hand capacitors to be used in the actual application or prototype testing. Under the schematic drawing, there is an important note. It states "Keep Crossover Frequency below 70 kHz, RTUNE should be 180 ohms or larger". This statement is meant to coach specifically for the PKX007 design. Each module schematic will have different coaching for the crossover frequency. When running the stability analysis, the user will use this coaching to ensure the loop is not set too aggressively (above 70 kHz) or too sluggish (far below 70 kHz).
PTM Published on: 2017-07-19