Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
key feat
Consistent for all the modules in the DLynx 2 family are the following attributes: easy and consistent design-in approach via the Power Module Wizard online tool, daisy chain any of the modules via PMBus within the DLynx 2 family, all have wide input voltage ranges and wide output programming range, the output voltage accuracy is +/-1% over the full operating temperature range, the digital readout accuracy of both the output voltage and the output current has been improved as compared to the previous generation of modules, and they are +/-2% and +/-5%, respectively. Another improvement from the previous generation is the addition of live digital temperature readout. All Pico and Micro modules also have an analog sibling module; same pinout and footprint, but “No Connects” where the original digital pads had resided. There is a cost savings for the analog versions.
PTM Published on: 2017-07-19