Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
EPS Heitec Sub-Rack Series Slide 9

When choosing a sub-rack solution from Wakefield Thermal it is important to note what packaging components are suitable to work with each other. All guide rail types are compatible with all sub-rack systems. The Ripac Easy and the Ripac ECO sub-components are only compliant with their respective family of sub-rack. The only exception to this rule is that the Ripac Eco’s horizontal rails are compatible with other families of sub-racks. The sub-components on the Vario Systems such as, Ripac Vario, Variio EMC, and Vario Mobile can all be used for each other.

PTM Published on: 2015-11-16