Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
TCR5AM LDO Slide 8

A major advantage of the TCR5AM is that it is a high output LDO in a small package. It can output up to 500 mA, despite being in a tiny 1.2 by 1.2 mm package. Toshiba’s packaging is thermally efficient, allowing it to dissipate heat quickly and safely without damaging the silicon. Furthermore, the N-channel MOSFET has very low resistance, which allows it to generate less heat in the first place.

PTM Published on: 2015-02-03