Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
Snap-Lock SMA Series 2
Tyco Electronics' Snap-Lock Series SMA plugs are designed to replace standard SMA plugs in existing or new designs. The problem with standard SMA plugs is that they have a threaded coupling mechanism which requires a specific torque (typically 7-10 in-lbs) for optimum connections. This process takes time, involves wear on the mating components and many times requires a separate tool to ensure that the required torque is achieved.
PTM Published on: 2011-11-07